GN 346 toggle pads are generally used for the transfer of clamping forces. They accommodate uneven or non-parallel surfaces and clamp without twisting the clamped parts.
The static loads indicated in the table were determined by a series of tests, wherein a limited number of toggle pads were subjected for a limited time to vertical static loads. At the values shown, a permanent deformation of the ball is almost impossible.
These toggle pads can also be used as leveling feet with a small foot diameter.
This article is RoHS-compliant in application of Annex III., which means it complies with EU Directive 2011/65/EU, including extension (2015/863/EU), for restricting the use of certain hazardous substances in electrical and electronic devices. The Directive regulates the use of hazardous substances in devices and components. The implementation in national law is summarily described with RoHS(Restriction of (the use of certain) hazardous substances)).
Weight: 0.044 lbs
If weight is not listed, please contact our Sales Department for additional information regarding weight. Phone: 800-877-8351