Detail | JW Winco Standard Parts

JW Winco Offers Safety Indexing Plungers with Push Button Click-Type Lock

GN 414.1 Metric Size, Steel, Safety Indexing Plungers

New GN 414.1 safety indexing plungers with click type lock are used when the plunger pin is to be briefly prevented from protruding. The safety lock on these RoHS compliant products can be unlocked only by exerting axial pressure on the red safety push button, with the plunger pin then returning to its starting position by spring force.

JW Winco, A Ganter Company, a leading supplier of standard industrial machine components, announced it now offers GN 414.1 Metric Size, Steel, Safety Indexing Plungers with Push Button Click-Type Lock and pin in the retracted position.

The GN 414.1 safety indexing plungers with click type lock are used when the plunger pin is to be briefly prevented from protruding. When the pin is retracted to its end position, the button engages with a clearly audible click. The safety lock on these RoHS compliant products can be unlocked only by exerting axial pressure on the red safety push button, with the plunger pin then returning to its starting position by spring force.

The plunger body and pin are made from steel with a black oxide finish and the plunger pin is hardened. The knob is technopolymer plastic with a matte black-gray color that is not removable, while the safety push button is also made from technopolymer plastic in matte red.

JW Winco offers an extensive selection of inch and metric size adjustable levers, cabinet U-handles, plastic and steel hinges and locking mechanisms, revolving and retractable handles, hand wheels, hand cranks, tube connection and conveyor components, inch and metric construction tubing, shock absorption mounts, leveling mounts, hand knobs, spring, ball and indexing plungers, jig, fixture and fastening components, retaining magnet assemblies, toggle clamps, metric casters and wheels, universal joints, oil sight glasses, and metric tools for the industrial and commercial equipment industries. JW Winco’s new website, with improved 3D CAD and online buying, is viewable at www.jwwinco.com.

JW Winco, which is ISO 9001:2008 certified, is located in New Berlin, Wisconsin, with sales locations in Canada and Mexico. For more information, contact JW Winco at 800-877-8351, by fax at 800-472-0670, on the Web at www.jwwinco.com, and via e-mail at sales@jwwinco.com.

Back

JW Winco Press Releases

Click below for press releases on new products or additions and extensions to our product range!

Go to the Press Releases

New Products

Click below to hear about our new products or new additions to our product range!

Go to New Products