J.W. Winco, Inc., a leading supplier of standard industrial machine components, announced it now offers GN 822.1 Metric Size, Stainless Steel Mini Indexing Plungers Lock-out and Non Lock-out Types, with Open Lock Mechanism.
The RoHS compliant indexing plungers feature small, compact dimensions, as they are designed for installation in thin walled sheet metal applications. Plungers are inserted into position by holding them by the knurled knob. The wrench flats on the lock nut are exposed when the pin is retracted, so that the plunger can be easily tightened by means of an open-end wrench.
The indexing plunger with the lock-out position is for applications that require the plunger pin to be retracted for an extended period of time.
The body, plunger, and spring are stainless steel, while the knob is matte black technopolymer plastic, not removable.
J.W. Winco offers an extensive selection of inch and metric size adjustable levers, cabinet U-handles, plastic and steel hinges and locking mechanisms, revolving and retractable handles, hand wheels, hand cranks, tube connection and conveyor components, inch and metric construction tubing, shock absorption mounts, leveling mounts, hand knobs, spring, ball and indexing plungers, jig, fixture and fastening components, retaining magnet assemblies, toggle clamps, metric casters and wheels, universal joints, oil sight glasses, and metric tools for the industrial and commercial equipment industries. J.W. Winco’s Web site catalog, with 3D CAD and online buying, is viewable at www.jwwinco.com.
For more information, contact J.W. Winco at 800-877-8351, by fax at 800-472-0670, on the Web at www.jwwinco.com, and via e-mail at sales@jwwinco.com.
Précédent