Detail | JW Winco Standard Parts

Extended Range of Ball Plungers Available from JW Winco

Ball-Plungers

New Ball Plungers for securing as well as for pressure and stand-off functions.

JW Winco, Inc., A Ganter Company, a leading supplier of standard industrial machine components, now has available GN 615.5 Ball Plungers in A4 Stainless Steel, with Ceramic Ball, GN 615.8 Ball Plungers in Stainless Steel or Steel, with Friction Bearing, with Slot, and GN 615.9 Ball Plungers in Stainless Steel or Steel, with Friction Bearing, with Internal Hexagon.

      All three versions of the ball plungers are used for securing as well as for pressure and stand-off functions. “The 615.5 stainless steel ball plungers are suitable for use in highly corrosive environments,” said John Winkler, CEO, Office of the President at JW Winco. “Plus, the ceramic ball is low wearing, anti-magnetic, and electrically insulating.”

      Versions 615.8 and 615.9 feature the ball mounted in a plastic friction bearing shell so as to be freely movable, which enables rolling and optimizes the securing characteristics. “Above all, this reduces wear on the mating part” Winkler said. “Another characteristic of these plungers is that the plastic friction bearing shell also acts as an electrical insulator.” Plastic shell temperature resistant up to 194 °F (90 °C).

Back

JW Winco Press Releases

Click below for press releases on new products or additions and extensions to our product range!

Go to the Press Releases

New Products

Click below to hear about our new products or new additions to our product range!

Go to New Products