Detail | JW Winco Standard Parts

New Hygienic Design Stainless Steel Cabinet "U" Handles

Hygienic Design Stainless Steel Cabinet U-Handles.

GN 429 Hygienic Design Cabinet "U" Handles sealed mounting surfaces enable fastening without dead spaces, while the high quality finish prevents adherence of dirt and facilitates cleaning.

JW Winco, Inc., A Ganter Company, a leading supplier of standard industrial machine components, announced the availability of GN 429 Hygienic Design Stainless Steel Cabinet "U" Handles.

The RoHS compliant cabinet “U“ handles are intended for use in hygiene areas. The sealed mounting surfaces enable fastening without dead spaces, while the high quality finish prevents adherence of dirt and facilitates cleaning. In addition, the process of manufacturing the handles through bending allows the production of special lengths in relatively small quantities.

The matte and polished handle is made of stainless steel, while the FDA compliant sealing ring is comprised of a blue hydrogenated acrylonitrile butadiene rubber that is temperature resistant -77° F (-25 °C) to + 302 °F (+ 150 °C).

JW Winco offers an extensive selection of inch and metric size adjustable levers, cabinet U-handles, plastic and steel hinges and locking mechanisms, revolving and retractable handles, hand wheels, hand cranks, tube connection and conveyor components, inch and metric construction tubing, shock absorption mounts, leveling mounts, hand knobs, spring, ball and indexing plungers, jig, fixture and fastening components, retaining magnet assemblies, toggle clamps, metric casters and wheels, universal joints, oil sight glasses, and metric tools for the industrial and commercial equipment industries. JW Winco’s new website, with improved 3D CAD and online buying, is viewable at www.jwwinco.com.

      JW Winco, which is ISO 9001:2008 certified, is located in New Berlin, Wisconsin, with sales locations in Canada and Mexico. For more information, contact JW Winco at 800-877-8351, by fax at 800-472-0670, on the Web at www.jwwinco.com, and via e-mail at sales@jwwinco.com.

Back

JW Winco Press Releases

Click below for press releases on new products or additions and extensions to our product range!

Go to the Press Releases

New Products

Click below to hear about our new products or new additions to our product range!

Go to New Products