JW Winco, Inc., A Ganter Company, a leading supplier of standard industrial machine components, announced it now offers GN 196 Aluminum Angle Connector Clamps in metric sizes. These clamps offer many more application opportunities within the expansive range of tube clamps currently offered.
The angle connector clamps, which are RoHS compliant, have clamping bores that are specially designed for JW Winco metric construction tubing Series GN 990, DIN 2391, DIN 2395 and DIN 2462 respectively. The connector clamp is comprised of aluminum and comes with either a powder coated black textured finish or a plain, matte shot-blast finish. The securing socket cap screws, nylon insert hex nuts, and set screws are all made of A2 / 304 stainless steel.
JW Winco offers an extensive selection of inch and metric size adjustable levers, cabinet U-handles, plastic and steel hinges and locking mechanisms, revolving and retractable handles, hand wheels, hand cranks, tube connection and conveyor components, inch and metric construction tubing, shock absorption mounts, leveling mounts, hand knobs, spring, ball and indexing plungers, jig, fixture and fastening components, retaining magnet assemblies, toggle clamps, metric casters and wheels, universal joints, oil sight glasses, and metric tools for the industrial and commercial equipment industries. JW Winco’s new website, with improved 3D CAD and online buying, is viewable at www.jwwinco.com.
JW Winco, which is ISO 9001:2008 certified, is located in New Berlin, Wisconsin, with sales locations in Canada and Mexico. For more information, contact JW Winco at 800-877-8351, by fax at 800-472-0670, on the Web at www.jwwinco.com, and via e-mail at sales@jwwinco.com.
Back
We are grateful for our customers, partners, suppliers and JW Winco team!
Our offices will be closed 12/24, 12/25, 12/31 and 1/1 in celebration of the holidays.