Detail | JW Winco Standard Parts

Metric Size Steel or Stainless Steel Spring Cotter Pins

Cotter Pins

Cotter Pins are used for the axial mounting of bolts and axles, as well as an anti-twist mechanism.

NEW BERLIN, WI -- J.W. Winco, Inc., a leading supplier of standard industrial machine components, announced it now offers GN 1024 Metric Size Steel or Stainless Steel Spring Cotter Pins.

The GN 1024 spring cotter pins, which are RoHS compliant, are used for the axial mounting of bolts and axles, as well as an anti-twist mechanism. Due to their double loop, spring cotter pins have a flatter spring characteristic and are therefore easier to install. Also, a retaining cable with a key ring can be attached to the double loop to safeguard the spring cotter pins against loss. The steel version is zinc plated with a blue passivated finish.

J.W. Winco offers an extensive selection of inch and metric size adjustable levers, cabinet U-handles, plastic and steel hinges and locking mechanisms, revolving and retractable handles, hand wheels, hand cranks, tube connection and conveyor components, inch and metric construction tubing, shock absorption mounts, leveling mounts, hand knobs, spring, ball and indexing plungers, jig, fixture and fastening components, retaining magnet assemblies, toggle clamps, metric casters and wheels, universal joints, oil sight glasses, and metric tools for the industrial and commercial equipment industries. J.W. Winco’s Web site catalog, with 3D CAD and online buying, is viewable at www.jwwinco.com.

For more information, contact J.W. Winco at 800-877-8351, by fax at 800-472-0670, on the Web at www.jwwinco.com, and via e-mail at sales@jwwinco.com.

Back

JW Winco Press Releases

Click below for press releases on new products or additions and extensions to our product range!

Go to the Press Releases

New Products

Click below to hear about our new products or new additions to our product range!

Go to New Products