J.W. Winco, Inc., a leading supplier of standard industrial machine components, announced it now offers WN 303 and WN 303.1 Nylon Plastic Adjustable Levers with Push Button, Threaded Stud Type, with either Steel or Stainless Steel Components.
Patented and made in the United States, the WN 300 adjustable hand levers with push button, which are also RoHS compliant, are the result of modern industrial design. All such levers have proven to be best wherever parts have to be clamped in a confined space or in a particular lever position.
The insert is connected to the hand lever via serrations that can easily be disengaged. Pulling the lever upward disengages the serrations, allowing it to be swiveled to the ideal clamping position. On releasing the lever, the serrations automatically re-engage. The nylon plastic levers have a maximum heat resistance of 150°C (230°F). In addition, special threads and stud lengths are available upon request.
The lever handle is glass fiber reinforced thermoplastic with a molded in metal insert and comes in black, orange, or gray. The push button is nylon plastic, available in black, orange, or gray, while the screw where the push button is mounted is made of stainless steel. The insert with threaded stud and spring is available in either steel, with a black oxide finish, or in stainless steel.
J.W. Winco offers an extensive selection of inch and metric size adjustable levers, cabinet U-handles, plastic and steel hinges and locking mechanisms, revolving and retractable handles, hand wheels, hand cranks, tube connection and conveyor components, inch and metric construction tubing, shock absorption mounts, leveling mounts, hand knobs, spring, ball and indexing plungers, jig, fixture and fastening components, retaining magnet assemblies, toggle clamps, metric casters and wheels, universal joints, oil sight glasses, and metric tools for the industrial and commercial equipment industries. J.W. Winco’s Web site catalog, with 3D CAD and online buying, is viewable at www.jwwinco.com.
For more information, contact J.W. Winco at 800-877-8351, by fax at 800-472-0670, on the Web at www.jwwinco.com, and via e-mail at sales@jwwinco.com.
BackWe are grateful for our customers, partners, suppliers and JW Winco team!
Our offices will be closed 12/24, 12/25, 12/31 and 1/1 in celebration of the holidays.