JW Winco, Inc., A Ganter Company, a leading supplier of standard industrial machine components, announced it now offers Stainless Steel Nylon Wheel Swivel Casters with Plate Mounting.
These swivel casters, which are RoHS compliant, have a load capacity range based on manual operation of 150-300kg. Featuring high abrasion and low rolling resistance, the swivel casters are also impact proof and corrosion resistant. They have a high chemical resistance to alcohol, salts, grease, and certain diluted acids and lyes, and are smooth running on even floors.
The bracket is a stainless steel 304 metal stamping with a high quality polished surface. It also has a double ball bearing race in the swivel head and a heavy-duty central king pin that secures the mounting plate to the swivel head. All metal parts including balls, central king pin, and axle material are also made of stainless steel.
The wheel is constructed of a quality, impact-resistant natural white nylon material, with a 70° Durometer Shore D Hardness.
JW Winco Stainless Steel Nylon Wheel Swivel Casters was featured in the February 2018 issues of Modern Materials Handling and Material Handling Product News magazines.
BackWe are grateful for our customers, partners, suppliers and JW Winco team!
Our offices will be closed 12/24, 12/25, 12/31 and 1/1 in celebration of the holidays.