NEW BERLIN, WI – JW Winco, Inc., A Ganter Company, a leading supplier of standard industrial machine components, announced it now offers GN 20 Leveling feet in Hygienic Design, with mounting holes.
These hygienic leveling feet with mounting holes are certified according to European Hygienic Engineering and Design Group guidelines, making them ideal for use in hygienic applications, as the bottom seal protects the area beneath the foot plate from dirt.
For this, the foot must be screwed on using the mounting holes and compressed accordingly. The sealing ring above the adjustment sleeve enables fastening without dead space. Due to the wiper or the ball seal, the moving components are sealed against the environment, while the finish prevents adherence of dirt and facilitates cleaning.
J.W. Winco offers an extensive selection of inch and metric size adjustable levers, cabinet U-handles, plastic and steel hinges and locking mechanisms, revolving and retractable handles, hand wheels, hand cranks, tube connection and conveyor components, inch and metric construction tubing, shock absorption mounts, leveling mounts, hand knobs, spring, ball and indexing plungers, jig, fixture and fastening components, retaining magnet assemblies, toggle clamps, metric casters and wheels, universal joints, oil sight glasses, and metric tools for the industrial and commercial equipment industries. J.W. Winco’s new website catalog, with improved 3D CAD and online buying, is viewable at www.jwwinco.com.
Click Here to view the GN 20 product page.
JW Winco, which is ISO 9001:2008 certified, is located in New Berlin, Wisconsin, with sales locations in Canada and Mexico. For more information, contact J.W. Winco at 800-877-8351, by fax at 800-472-0670, on the Web at www.jwwinco.com, and via e-mail at sales@jwwinco.com.
BackWe are grateful for our customers, partners, suppliers and JW Winco team!
Our offices will be closed 12/24, 12/25, 12/31 and 1/1 in celebration of the holidays.