These GN 414 Metric Size, Stainless Steel, Safety Indexing Plungers with pin in protruding position are RoHS compliant safety-indexing plungers are used when the inadvertent retraction of the plunger pin is to be prevented.
The Protruding Plunger Pin is first locked and may be unlocked for pulling only by exerting axial pressure on the red safety push-button. The safety lock engages in the front end position, i.e. automatically if the indexing pin protrudes, with the locking mechanism housed fully in the operating button and protected from malfunctions. The specified axial load bearing capacity refers to the locking force of the bolt against inadvertent operation, which must not be exceeded.
Temperature resistant to 80° C (176° F), the plunger body and pin are made of stainless steel, while the pin is chemically nickel-plated. The knob is technopolymer plastic in matte black-gray and is not removable. The safety push button is also made of technopolymer plastic and is a matte red color.
Click here to go to the product page of the GN 414 Metric Size, Stainless Steel, Safety Indexing Plungers with pin in protruding position.
J.W. Winco offers an extensive selection of inch and metric size adjustable levers, cabinet U-handles, plastic and steel hinges and locking mechanisms, revolving and retractable handles, hand wheels, hand cranks, tube connection and conveyor components, inch and metric construction tubing, shock absorption mounts, leveling mounts, hand knobs, spring, ball and indexing plungers, jig, fixture and fastening components, retaining magnet assemblies, toggle clamps, metric casters and wheels, universal joints, oil sight glasses, and metric tools for the industrial and commercial equipment industries. J.W. Winco’s Web site catalog, with 3D CAD and online buying, is viewable at www.jwwinco.com.
For more information, contact J.W. Winco at 800-877-8351, by fax at 800-472-0670, on the Web at www.jwwinco.com, and via e-mail at sales@jwwinco.com.
Back
We are grateful for our customers, partners, suppliers and JW Winco team!
Our offices will be closed 12/24, 12/25, 12/31 and 1/1 in celebration of the holidays.