Detail | JW Winco Standard Parts

Indexing Plungers with Removable Pin, Lock-Out or Non Lock-Out Type

The RoHS compliant GN 817.8 indexing plungers are designed so that special versions of the indexing pins can be made economically in smaller unit quantities. If required, the indexing pins can be machined or made by the user. They are assembled with a countersunk screw and can therefore be assembled several times. All parts are supplied individually as a disassembled set.

One version of the indexing plungers is used for applications where the plunger has to stay in its retracted position. To achieve this, the knob is rotated by 90° degrees after being retracted, as a notch keeps the plunger in this position. The maximum heat resistance of the matte black technopolymer nylon plastic hand knob, which is not removable, is 110°C (230°F).

The threaded body and lock nut are steel with a black oxide finish, while the plunger pin and countersunk screw are stainless steel.

J.W. Winco offers an extensive selection of inch and metric size adjustable levers, cabinet U-handles, plastic and steel hinges and locking mechanisms, revolving and retractable handles, hand wheels, hand cranks, tube connection and conveyor components, inch and metric construction tubing, shock absorption mounts, leveling mounts, hand knobs, spring, ball and indexing plungers, jig, fixture and fastening components, retaining magnet assemblies, toggle clamps, metric casters and wheels, universal joints, oil sight glasses, and metric tools for the industrial and commercial equipment industries. J.W. Winco’s website catalog, with 3D CAD and online buying, is viewable at www.jwwinco.com.

For more information, contact J.W. Winco at 800-877-8351, by fax at 800-472-0670, on the Web at www.jwwinco.com, and via e-mail at sales@jwwinco.com.

Back

JW Winco Press Releases

Click below for press releases on new products or additions and extensions to our product range!

Go to the Press Releases

New Products

Click below to hear about our new products or new additions to our product range!

Go to New Products