JW Winco, Inc., A Ganter Company, a leading supplier of standard industrial machine components, announced it now offers <link en-us/products/quick-finder/GN-342.1-Steel-Vibration-Dampening-Leveling-Mounts-Tapped-Type?q=342 _blank>GN 342.1 Tapped </link>/ <link en-us/products/quick-finder/GN-342.2-Steel-Vibration-Dampening-Leveling-Mounts-Threaded-Stud-Type?q=342 _blank>342.2 Threaded Stud</link>, Steel Vibration Dampening Leveling Mounts in Metric Sizes.
The specified load for these RoHS compliant leveling mounts features a recommendation up to the point the dampening element that can be permanently subjected. This static load equals a thrust on the area, at which the dampening material reaches its optimum dynamic dampening ability. The elastomer of the dampening element is oil resistant and has an operating range from -30° C (-22° F) to +70° C (158° F).
The leveling mounts, which cannot be disassembled, feature a base, tapped socket or threaded stud, hex nut (hex nut is included with threaded stud version), that are steel, with a zinc plated, blue passivated finish, while the dampening element is anti-slip elastomer material in gray and glued to the base.
JW Winco offers an extensive selection of inch and metric size adjustable levers, cabinet U-handles, plastic and steel hinges and locking mechanisms, revolving and retractable handles, hand wheels, hand cranks, tube connection and conveyor components, inch and metric construction tubing, shock absorption mounts, leveling mounts, hand knobs, spring, ball and indexing plungers, jig, fixture and fastening components, retaining magnet assemblies, toggle clamps, metric casters and wheels, universal joints, oil sight glasses, and metric tools for the industrial and commercial equipment industries. JW Winco’s new website, with improved 3D CAD and online buying, is viewable at www.jwwinco.com.
JW Winco, which is ISO 9001:2008 certified, is located in New Berlin, Wisconsin, with sales locations in Canada and Mexico. For more information, contact JW Winco at 800-877-8351, by fax at 800-472-0670, on the Web at www.jwwinco.com, and via e-mail at sales@jwwinco.com.
BackAttention Valued Customer,
Beginning April 14, 2025, we will implement a price adjustment. Some items will have a price decrease, while others will increase. The adjustment helps ensure our commitment to providing our customers with the best products and services.
We will honor current published prices through April 13, 2025.
Customers with pricing agreements will not be effected until annual pricing is reviewed.