JW Winco, Inc., A Ganter Company, a leading supplier of standard industrial machine components, announced the offering of GN 2342 Stainless Steel Assembly Pins.
These RoHS compliant assembly pins are characterized by their use in diverse applications. Depending on the requirement, there are three washer types to choose from, which place the bolt in an axial position in its insertion direction. The washer with eyelet (Type E), the assembly pin and a corresponding spring cotter pin can be secured to prevent loss using a retaining cable or ball chain. The washer with mounting shackle (Types L) simultaneously acts as loss protection and anti-rotation protection.
The assembly pin and washer are stainless steel, as is the countersunk screw, which is not removable and loctited in place.
JW Winco offers an extensive selection of inch and metric size adjustable levers, cabinet U-handles, plastic and steel hinges and locking mechanisms, revolving and retractable handles, hand wheels, hand cranks, tube connection and conveyor components, inch and metric construction tubing, shock absorption mounts, leveling mounts, hand knobs, spring, ball and indexing plungers, jig, fixture and fastening components, retaining magnet assemblies, toggle clamps, metric casters and wheels, universal joints, oil sight glasses, and metric tools for the industrial and commercial equipment industries. JW Winco’s new website, with improved 3D CAD and online buying, is viewable at www.jwwinco.com.
JW Winco, which is ISO 9001:2008 certified, is located in New Berlin, Wisconsin, with sales locations in Canada and Mexico. For more information, contact JW Winco at 800-877-8351, by fax at 800-472-0670, on the Web at www.jwwinco.com, and via e-mail at sales@jwwinco.com.
BackWe are grateful for our customers, partners, suppliers and JW Winco team!
Our offices will be closed 12/24, 12/25, 12/31 and 1/1 in celebration of the holidays.