JW Winco, Inc., A Ganter Company, a leading supplier of standard industrial machine components, announced the introduction of GN 5435 Hygienic Design Stainless Steel Star Knobs.
These specially designed Star Knobs, which are RoHS compliant, are intended for use in hygiene areas. The sealed mounting surface enables fastening without dead spaces, as the high quality finish and the large corner radii prevent adherence of dirt and facilitates cleaning.
The matte and polished stainless-steel knob has a FDA compliant sealing ring made from a blue hydrogenated acrylonitrile butadiene rubber that is temperature resistant -77° F (-25 °C) to + 302 °F (+ 150 °C).
JW Winco offers an extensive selection of inch and metric size adjustable levers, cabinet U-handles, plastic and steel hinges and locking mechanisms, revolving and retractable handles, hand wheels, hand cranks, tube connection and conveyor components, inch and metric construction tubing, shock absorption mounts, leveling mounts, hand knobs, spring, ball and indexing plungers, jig, fixture and fastening components, retaining magnet assemblies, toggle clamps, metric casters and wheels, universal joints, oil sight glasses, and metric tools for the industrial and commercial equipment industries. JW Winco’s new website, with improved 3D CAD and online buying, is viewable at www.jwwinco.com.
JW Winco, which is ISO 9001:2008 certified, is located in New Berlin, Wisconsin, with sales locations in Canada and Mexico. For more information, contact JW Winco at 800-877-8351, by fax at 800-472-0670, on the Web at www.jwwinco.com, and via e-mail at sales@jwwinco.com.
BackWe are grateful for our customers, partners, suppliers and JW Winco team!
Our offices will be closed 12/24, 12/25, 12/31 and 1/1 in celebration of the holidays.