Detail | JW Winco Standard Parts

JW Winco Offers Latches with Safety Function

GN-115.9-Latches-with-Safety-Function-Zinc-Die-Casting-Operation-with-Key-not-Lockable

New GN 115.9 Latches with Safety Function

JW Winco, Inc., A Ganter Company, a leading supplier of standard industrial machine components, has available GN 115.9 Latches with Safety Function, Zinc Die Casting, Operation with Key, not Lockable.

These latches, which are RoHS compliant, have a push-to-turn safety function. In the two end positions, the lock secures the spindle in place. The device can be turned 90° only when the operating element is pressed down, which releases the safety pin from the locked position. This feature protects the lock reliably from moving on its own or as the result of vibrations.

The beveled edges on the lock make closing the door easy. The 15 different offsets allow the latch distance A to be set between 4 and 32 mm.

The lock housing is Zinc die cast with a zinc plated finish, while the locating ring is plastic coated black with a textured finish. All other parts are steel zinc plated, with a blue passivated finish. The latches are delivered with the lock enclosed separately.

Back

New Products

You know our products but you're looking for new products or new additions to our product range?

Go to New Products