JW Winco Offers Stainless Steel Folding Handles
JW Winco, Inc., A Ganter Company, a leading supplier of standard industrial machine components, now has available GN 425.9 Folding Handles in Stainless Steel.
The GN 425.9 stainless steel folding handles are used for lifting and pulling where the handle must only protrude a short distance in the resting position. “Two versions of the folding handles are available for side lifting, as they have a 90° limit stop,” said John Winkler, CEO, Office of the President at JW Winco. “If the application requires lifting from above, there are two other options where the handle can lift up and fold freely 180°.”
The retaining springs keep the handle in any position. “This keeps the handle in a position that can be easily accessed and prevents noise as a result of vibration in the resting position,” Winkler said. “The handle and the retaining springs are secured by mounting the handle base to the surface either from the front, back, or welding it in place.”
Designed for use in the packaging, equipment case manufacturing, material handling, and transportation industries, the finish is either matte, shot-blasted or powder coated in black with a textured finish. The folding handle has a matte, shot-blasted finish.
For a folding handle with a recessed tray see our GN 425.8 series, for a folding handle with threaded stems see our GN 425.2 series.
Back