Videos | JW Winco Standard Parts

Company and Product Videos

JW Winco's 45 Year Anniversary

JW Winco's 45 Year Anniversary

Hear from our President, Mark Winkler, how his Mom and Dad started the business in 1978 and how he plans to carry the torch forward. We are grateful to celebrate 45 years of success and honored to help customers be the best they can be.

Company Video

Company Video

JW Winco is leading in the development, production and distribution of standard parts for the entire industry. The comprehensive range of products sets standards across all branches and provides our customers with a one-stop shopping experience. Quality, service and availability are therefore guaranteed, no matter the location.

Wheels and Casters

Wheels and Casters

Wheels and casters are indispensable standard parts in many areas of daily life and in industry. From workshops to offices and warehouses, they provide mobility and make it easier to move goods and equipment around.

Sensor Holders GN 801.3 / GN 801.4

Sensor Holders GN 801.3 / GN 801.4

Sensor holders GN 801.3 / GN 801.4 are designed as accessories for GN 810 and GN 820 series toggle clamps and enable contactless monitoring of the clamping positions using an inductive sensor.

Standard Connectors GN 20i

Standard Connectors GN 20i

Standard connectors GN 20i fasten aluminum profiles at right angles and secure them against twisting. This requires machining of both profiles. The internal thread can be cut directly into the end face profile holes.

Central Screws GN 21b

Central Screws GN 21b

Central screws GN 21b connect aluminum profiles at right angles. Only one profile has to be machined. The thread in the end face profile hole is formed by the central screw itself. The self-forming thread should be lubricated to simplify assembly.

Universal Connectors GN 22i

Universal Connectors GN 22i

Universal connectors GN 22i fasten aluminum profiles together at right angles and, when used in pairs, secure them against twisting. Only one profile has to be machined.

Automatic Connectors GN 23b - Coding R

Automatic Connectors GN 23b - Coding R

Automatic connectors GN 23b fasten aluminum profiles together at right angles. Machining of the profile is not necessary. The connection can be freely positioned and slid along the slot.

Automatic Connectors GN 23b - Coding S

Automatic Connectors GN 23b - Coding S

Automatic connectors GN 23b fasten aluminum profiles together on the end faces to extend them while securing them against twisting. Machining of the profile is not necessary.

Automatic Connectors GN 23i - Coding R

Automatic Connectors GN 23i - Coding R

Automatic connectors GN 23i fasten aluminum profiles together at right angles. Machining of the profile is not necessary. The connection can be freely positioned and slid along the slot.

Automatic Connectors GN 23i - Coding S

Automatic Connectors GN 23i - Coding S

Automatic connectors GN 23i fasten aluminum profiles together on the end faces to extend them while securing them against twisting. Machining of the profile is not necessary.

Quick Release Connectors GN 25b

Quick Release Connectors GN 25b

Quick release connectors GN 25b fasten aluminum profiles together at right angles. Only one profile has to be machined.

Bolt Connectors GN 26b

Bolt Connectors GN 26b

Bolt connectors GN 26b fasten aluminum profiles at right angles and secure them against twisting. Only one profile has to be machined.

Angle Connectors GN 32i - Identification no. 1

Angle Connectors GN 32i - Identification no. 1

Angle connectors GN 32i fasten aluminum profiles together at right angles and are primarily used for creating corner braces at 45° angles.

Angle Connectors GN 32i - Identification no. 2

Angle Connectors GN 32i - Identification no. 2

Angle connectors GN 32i fasten aluminum profiles together at right angles and are primarily used for creating corner braces at 45° angles.

Cube Connectors GN 33b

Cube Connectors GN 33b

Cube connectors GN 33b fasten two or three aluminum profiles together on their end faces, at right angles and with anti-twist protection. Machining of the profile is not necessary.

Cabinet U-Handles LED Illuminated EN 6284

Cabinet U-Handles LED Illuminated EN 6284

JW Winco's innovative cabinet u-handles EN 6284 have integrated LED handle lighting, which serves as a status indicator. This power switch functionality lets you obtain various colors by combining red, blue, and green lights. The EN 6284 comes with the option of cable or connector. Complementary cabinet u-handles without switching functions are available as EN 6284.1.

Threaded Lifting Pins

Threaded Lifting Pins

JW Winco quick release, threaded lifting pins GN 1133 and GN 1135 are support elements designed for quick and easy use. Pressing the operating button unlocks the threaded segments, allowing the pin to be moved in or out of the mounting thread. This eliminates the time-consuming process of screwing in or out encountered with typical lifting gear, such as lifting eye bolts.

Indexing Plungers GN 817.7

Indexing Plungers GN 817.7

Indexing plungers GN 817.7 with pneumatic operation can be easily and securely integrated into automated processes and can be positioned at locations where hand operation of the indexing plunger is not possible. Thanks to the material used, the indexing plungers are also suitable for more aggressive environments.

GN 7237 Stainless Steel-Multiple-joint Hinge

GN 7237 Stainless Steel-Multiple-joint Hinge

Overview video and application example of the GN 7237 Multiple-Joint Hinges

Ball Shaped Door Catches EN 450

Ball Shaped Door Catches EN 450

Ball shaped door catches EN 450 were designed for use with both shutter doors and sliding doors. The ball shaped door catch consists of a catch body to be fixed to a frame and a ball to be fixed to a door. Under specific tests, the catch showed constant performances for more than 20.000 cycles.

Hinges with Integrated Switch EN 239.4

Hinges with Integrated Switch EN 239.4

Hinges with integrated switch EN 239.4 are designed for monitoring guard doors and covers of machines and production equipment. Opening the door activates the switch contacts, which then interrupts a protective circuit via a break contact (NC) and at the same time signal the door opening by closing a make-contact element (NO).

 

Safety Hinges EN 239.6 - type of assembly

Safety Hinges EN 239.6 - type of assembly

Hinges with integrated safety switch EN 239.6 are designed for monitoring guard doors and covers of machines and production equipment. Opening the door activates the switch contacts, which then interrupts a protective circuit via a break contact (NC) and at the same time signal the door opening by closing a make-contact element (NO).

Safety Hinges EN 239.6 - operating features

 Safety Hinges EN 239.6 - operating features

Hinges with integrated safety switch EN 239.6 are designed for monitoring guard doors and covers of machines and production equipment. Opening the door activates the switch contacts, which then interrupts a protective circuit via a break contact (NC) and at the same time signal the door opening by closing a make-contact element (NO).

 

Position Indicators EN 954 and EN 9054

Position Indicators EN 954 and EN 9054

Digital Position Indicators EN 954 and EN 9054 from JW Winco

Position Indicator EN 9153 and Control Unit EN 9150

Position Indicator EN 9153 and Control Unit EN 9150

Position Indicator EN 9153 and Control Unit EN 9150 from JW Winco.

 

Roller Tracks and Accessories

Roller Tracks and Accessories

Roller track assemblies and ball rail assemblies allow linear movement on rollers and enable conveyed materials to move in every direction on ball tracks. In industrial production facilities, they apply to linked process lines, packaging tables, and flow racks.

Panel Support Clamp EN 649

 Panel Support Clamp EN 649

The panel support clamp EN 649 complies with Machinery Directive 2006/42/EG (captivity of the mounting element when open).

The two clamping jaws remain connected when open by means of a pin sliding into a groove. The clamping screw (M5) is also captive.

 

Breather Caps and Breather Valve Caps

Breather Caps and Breather Valve Caps

Breather caps and breather valve caps let in clean air for equalized pressure or volume in the space between a container’s interior and its surroundings. If it is necessary to avoid any impure particles or media from entering, additional membranes and filters are available.

 

Rotary Toggle Latches EN 5630

Rotary Toggle Latches EN 5630

Rotary toggle latches EN 5630 allow doors, covers and hatches to be closed and locked.

Fluid Level Indicator EN 654 EN 654.1 and Assembly Set EN 654.2

Fluid Level Indicator EN 654 EN 654.1 and Assembly Set EN 654.2

Fluid Level Indicator EN 654,EN 654.1 and Assembly Set EN 654.2 from JW Winco.

 

Torque Limiting Knurled Knobs EN 5910

Torque Limiting Knurled Knobs EN 5910

Torque limiting knurled knobs EN 5910 are used when the manually applied torque is to be limited. The torque limit can be set between 0.2 Nm and 1 Nm.

Magnetic Measuring Systems and Bands

Magnetic Measuring Systems and Bands

“Measure once, cut once” with Magnetic measuring systems EN 7110 and magnetic bands EN 7110.2. Together these products form a complete system for length and angle measurement suitable for applications requiring frequent adjustments, such as cutting and trimming stations.

Standard Parts made of Detectable Plastics

Standard Parts made of Detectable Plastics

Visually detectable standard parts are made of a blue plastic. The striking color makes them particularly visible to the human eye and, perhaps more importantly, to optical monitoring systems.

Pneumatic Fastening Clamps

Pneumatic Fastening Clamps

Pneumatic clamps allow automation of the manual clamping action of standard toggle clamps, opening up new applications. They are actuated by compressed air and can be used to securely clamp parts remotely by the push of a button. If the pressure fails, the pneumatic clamp remains closed.

Quick Release Couplings GN 1050

Quick Release Couplings GN 1050

GN 1050 quick release couplings, position and connect components without tools using inserts GN 1050.1 for a tight and repeatable fit.
Flanges GN 1050.2 are available as an accessory for the assembly of couplings and studs, and provide additional attachment options.

Clamping Knobs with Indexing Plunger

Clamping Knobs with Indexing Plunger

GN 7336.7 clamping knobs with indexing plunger are used for positioning, securing and clamping adjusting elements simultaneously.

Clamping Knobs with Indexing Plunger

Clamping Knobs with Indexing Plunger

GN 7336.8 clamping knobs with indexing plunger are used for positioning, securing and clamping adjusting elements simultaneously.

Standard Parts in Hygienic Design Leveling feet GN 20

Standard Parts in Hygienic Design Leveling feet GN 20

Clamping Levers with Eccentrical Cam

Clamping Levers with Eccentrical Cam

GN 927 clamping levers with eccentrical cam are used for rapid clamping and releasing operations. In contrast to a clamping operation utilizing only threads and a lateral force, these levers permit torque-free clamping via a combined downward vertical and cam actuated motion.

Stop Bolts

Stop Bolts

GN 251.2 stop bolts are supplied with a hardened spherical head that serves as an end stop. The two hexagon nuts allow exact positioning with counter-locking. When the workpiece contacts the bolt head, the built-in limit switch transmits an electrical control signal.

Telescopic Slides

Telescopic Slides

Telescopic slides are used in production facilities and industrial machines as simple, economical sliding shelves with a variety of possible fittings. They include partial, full, and overextension slides.

Torque Limiting Knurled Knobs GN 3663

Torque Limiting Knurled Knobs GN 3663

GN 928 Shaft Clamping Units / GN 928.1 Assembly Tools

GN 928 Shaft Clamping Units / GN 928.1 Assembly Tools

With GN 928 shaft clamping units, round workpieces from 6 to 125 mm can be rapidly, accurately and economically clamped.

Leveling elements GN 355

Leveling elements GN 355

Spring Plungers

Spring Plungers

Spring plungers use pressure pins or spring-loaded balls to index, clamp, or lock components in place. The spring-loaded devices use a friction lock in V-blocks and centering holes to position components.

Edge Protection Profiles

Edge Protection Profiles

Edge protections and edge protection seal profiles cover the sharp edges of panels and sheet metal to prevent damage. Hatches, flaps, and doors can be sealed with edge protection that have a seal profile.

 

Ball Lock Pins #lockingpins

Ball Lock Pins #lockingpins

Ball lock pins provide a quick, easy way to connect, secure, and affix various components that have a hole. The axial lock can be released by pressing a release button.

Application positioning elements GN 200, GN 215, GN 700

Application positioning elements GN 200, GN 215, GN 700

How to Download 2D & 3D CAD Files

How to Download 2D & 3D CAD Files

This tutorial will show you how to download quickly and easily CAD files from our website for free.

Overview of JW Winco

Overview of JW Winco

J.W. Winco, Inc. is profiled on this video that aired on the Fox News Business Channel show "Manufacturing Marvels" on April 9, 2013. The two-minute video explores the company's product line of inch and metric standard parts for industry, as well as its services, facilities, and website.