Retractable handles transmit manual operating forces, while their rotating cylindrical handles prevent swiveling or rotating movements from being transmitted back to the handle, such as from handwheels or cranks. The cylindrical grip is also designed to fold in at its attachment point so that it only
Retractable handles transmit manual operating forces, while their rotating cylindrical handles prevent swiveling or rotating movements from being transmitted back to the handle, such as from handwheels or cranks. The cylindrical grip is also designed to fold in at its attachment point so that it only sticks out during use, making for perfect handling.
Attention Valued Customer,
Beginning April 14, 2025, we will implement a price adjustment. Some items will have a price decrease, while others will increase. The adjustment helps ensure our commitment to providing our customers with the best products and services.
We will honor current published prices through April 13, 2025.
Customers with pricing agreements will not be effected until annual pricing is reviewed.